InspectionImportDmisBuilder Class¶
-
class
NXOpen.CAM.
InspectionImportDmisBuilder
¶ Bases:
NXOpen.Builder
Inspection Import Dmis dialog builder
To create a new instance of this class, use
NXOpen.CAM.InspectionOperationCollection.CreateImportDmisBuilder()
New in version NX11.0.1.
Properties¶
Property | Description |
---|---|
DmisFile | Returns or sets the dmis file |
GeomTol | Returns or sets the geometry tolerance |
McsCsys | Returns or sets the tag of the Csys to use as the MCS when importing the DMIS |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ImportDmis | Import Dmis file |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
DmisFile¶
-
InspectionImportDmisBuilder.
DmisFile
¶ Returns or sets the dmis file
-------------------------------------
Getter Method
Signature
DmisFile
Returns: Return type: str New in version NX11.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
DmisFile
Parameters: filename (str) – New in version NX11.0.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
GeomTol¶
-
InspectionImportDmisBuilder.
GeomTol
¶ Returns or sets the geometry tolerance
-------------------------------------
Getter Method
Signature
GeomTol
Returns: Return type: float New in version NX11.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
GeomTol
Parameters: geomTol (float) – New in version NX11.0.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
McsCsys¶
-
InspectionImportDmisBuilder.
McsCsys
¶ Returns or sets the tag of the Csys to use as the MCS when importing the DMIS
-------------------------------------
Getter Method
Signature
McsCsys
Returns: Return type: NXOpen.CoordinateSystem
New in version NX11.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
McsCsys
Parameters: mcsTag ( NXOpen.CoordinateSystem
) –New in version NX11.0.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
ImportDmis¶
-
InspectionImportDmisBuilder.
ImportDmis
¶ Import Dmis file
Signature
ImportDmis()
New in version NX11.0.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Validate¶
-
InspectionImportDmisBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.