InspectionGraphicalReportOutputBuilderOutputFormatType Enumeration

NXOpen.CAM.InspectionGraphicalReportOutputBuilder.OutputFormatType is an alias for NXOpen.CAM.InspectionGraphicalReportOutputBuilderOutputFormatType

class NXOpen.CAM.InspectionGraphicalReportOutputBuilderOutputFormatType

Bases: object

the output format type

Enum Members

Enum Member Enum Member Description
Html
Pdf
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.