InspectionCylinderFeatureBuilder Class¶
-
class
NXOpen.CAM.
InspectionCylinderFeatureBuilder
¶ Bases:
NXOpen.CAM.OperationBuilder
Represents a CMM Inspection Cylinder Feature builder
To create a new instance of this class, use
NXOpen.CAM.InspectionOperationCollection.CreateInspectionCylinderFeatureBuilder()
New in version NX7.0.0.
Properties¶
Property | Description |
---|---|
AxisDirectionI | Returns or sets the axis direction vector I component |
AxisDirectionJ | Returns or sets the axis direction vector J component |
AxisDirectionK | Returns or sets the axis direction vector K component |
AxisExtrapolationModeBuilder | Returns the Axis Extrapolation Mode Builder |
AxisVector | Returns or sets the cylinders axis vector |
BasePointX | Returns or sets the base point X coordinate |
BasePointY | Returns or sets the base point Y coordinate |
BasePointZ | Returns or sets the base point Z coordinate |
ChannelName | Returns or sets the channel’s name |
CsysReferenceType | Returns or sets the coordinate system reference type |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
CylinderCircleFitModeBuilder | Returns the Cylinder Circle Fitting Mode Builder |
Description | Returns or sets the description |
Diameter | Returns or sets the cylinder diameter |
EndOfPath | Returns the end event builder |
EndUdeSet | Returns the end ude set |
ExtentType | Returns or sets the extent type |
Geometry | Returns the geometry builder |
GougeChecking | Returns or sets the gouge checking flag |
HoleAxisType | Returns or sets the Hole Axis Type |
HoleDepth | Returns the max depth distance builder |
HoleDepthType | Returns or sets the Hole Depth Type |
InnerOuterType | Returns or sets the inspection feature inner/outer type (hole/pin) |
LayoutAndLayer | Returns the Layer and Layout |
Length | Returns or sets the length of the cylinder |
MotionOutputBuilder | Returns the motion output builder |
Name | Returns or sets the name |
Notes | Returns the notes builder |
OptimizationBasedOn | Returns or sets the optimization based on in operation |
OptimizationDistanceMethod | Returns or sets the optimization distance method in operation |
OptimizationLevel | Returns or sets the optimization level in operation |
OptimizationMethod | Returns or sets the optim method |
PathDisplayOptions | Returns the path display options builder |
PostToolPathExit | Returns or sets the environment variable that points to the post tool path generation library which has the exit |
RetractDistance | Returns the Retract Distance builder (inheritable double) |
RetractDistanceOnToolAxisChange | Returns the Retract Distance on Tool Axis Change builder (inheritable double) |
SafeClearance | Returns the safe clearance builder |
SelectToolFlag | Returns or sets the user selected tool |
SelectedCylinder | Returns the selected cylinder |
SelectedGeometry | Returns the selected cylinder geometry |
StartOfPath | Returns the start event builder |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
ToolChangeSetting | Returns the tool change builder |
ToolPathEditor | Returns the Tool Path Editor Builder |
ToolPathSplitParametersBuilder | Returns the tool path split Parameters |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
FlipAxisDirection | Flips the cylinder inspection feature axis direction vector |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCustomizableItemBuilder | Returns the customizable item builder for the given customizable item name |
GetCustomizableItemNames | Returns the names for all customizable item ids |
GetHoleAxisValues | Get the Hole Axis values |
GetObject | Returns the object currently being edited by this builder. |
SetHoleAxisValues | Set the Hole Axis values |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateAxisDirection | Updates cylinder inspection feature axis direction vector based on selected vector |
UpdateParams | Updates cylinder inspection feature characteristic parameters based on selected geometry |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AxisDirectionI¶
-
InspectionCylinderFeatureBuilder.
AxisDirectionI
¶ Returns or sets the axis direction vector I component
-------------------------------------
Getter Method
Signature
AxisDirectionI
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AxisDirectionI
Parameters: axisDirectionI (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
AxisDirectionJ¶
-
InspectionCylinderFeatureBuilder.
AxisDirectionJ
¶ Returns or sets the axis direction vector J component
-------------------------------------
Getter Method
Signature
AxisDirectionJ
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AxisDirectionJ
Parameters: axisDirectionJ (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
AxisDirectionK¶
-
InspectionCylinderFeatureBuilder.
AxisDirectionK
¶ Returns or sets the axis direction vector K component
-------------------------------------
Getter Method
Signature
AxisDirectionK
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AxisDirectionK
Parameters: axisDirectionK (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
AxisExtrapolationModeBuilder¶
-
InspectionCylinderFeatureBuilder.
AxisExtrapolationModeBuilder
¶ Returns the Axis Extrapolation Mode Builder
-------------------------------------
Getter Method
Signature
AxisExtrapolationModeBuilder
Returns: Return type: NXOpen.CAM.InspectionAxisExtrapolationModeBuilder
New in version NX9.0.0.
License requirements: None.
AxisVector¶
-
InspectionCylinderFeatureBuilder.
AxisVector
¶ Returns or sets the cylinders axis vector
-------------------------------------
Getter Method
Signature
AxisVector
Returns: Return type: NXOpen.Direction
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AxisVector
Parameters: axisVector ( NXOpen.Direction
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
BasePointX¶
-
InspectionCylinderFeatureBuilder.
BasePointX
¶ Returns or sets the base point X coordinate
-------------------------------------
Getter Method
Signature
BasePointX
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BasePointX
Parameters: basePointX (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
BasePointY¶
-
InspectionCylinderFeatureBuilder.
BasePointY
¶ Returns or sets the base point Y coordinate
-------------------------------------
Getter Method
Signature
BasePointY
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BasePointY
Parameters: basePointY (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
BasePointZ¶
-
InspectionCylinderFeatureBuilder.
BasePointZ
¶ Returns or sets the base point Z coordinate
-------------------------------------
Getter Method
Signature
BasePointZ
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BasePointZ
Parameters: basePointZ (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
CsysReferenceType¶
-
InspectionCylinderFeatureBuilder.
CsysReferenceType
¶ Returns or sets the coordinate system reference type
-------------------------------------
Getter Method
Signature
CsysReferenceType
Returns: Return type: NXOpen.CAM.CamInspectionOperationCsysreferencetypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CsysReferenceType
Parameters: csysReferenceType ( NXOpen.CAM.CamInspectionOperationCsysreferencetypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
CylinderCircleFitModeBuilder¶
-
InspectionCylinderFeatureBuilder.
CylinderCircleFitModeBuilder
¶ Returns the Cylinder Circle Fitting Mode Builder
-------------------------------------
Getter Method
Signature
CylinderCircleFitModeBuilder
Returns: Return type: NXOpen.CAM.InspectionCylinderCircleFitModeBuilder
New in version NX9.0.0.
License requirements: None.
Diameter¶
-
InspectionCylinderFeatureBuilder.
Diameter
¶ Returns or sets the cylinder diameter
-------------------------------------
Getter Method
Signature
Diameter
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Diameter
Parameters: diameter (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ExtentType¶
-
InspectionCylinderFeatureBuilder.
ExtentType
¶ Returns or sets the extent type
-------------------------------------
Getter Method
Signature
ExtentType
Returns: Return type: NXOpen.CAM.CamInspectionOperationExtenttypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExtentType
Parameters: extentType ( NXOpen.CAM.CamInspectionOperationExtenttypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
InnerOuterType¶
-
InspectionCylinderFeatureBuilder.
InnerOuterType
¶ Returns or sets the inspection feature inner/outer type (hole/pin)
-------------------------------------
Getter Method
Signature
InnerOuterType
Returns: Return type: NXOpen.CAM.CamInspectionOperationInneroutertypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InnerOuterType
Parameters: innerOuterType ( NXOpen.CAM.CamInspectionOperationInneroutertypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Length¶
-
InspectionCylinderFeatureBuilder.
Length
¶ Returns or sets the length of the cylinder
-------------------------------------
Getter Method
Signature
Length
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Length
Parameters: length (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Name¶
-
InspectionCylinderFeatureBuilder.
Name
¶ Returns or sets the name
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name
Parameters: name (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SelectedCylinder¶
-
InspectionCylinderFeatureBuilder.
SelectedCylinder
¶ Returns the selected cylinder
-------------------------------------
Getter Method
Signature
SelectedCylinder
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.0.0.
License requirements: None.
SelectedGeometry¶
-
InspectionCylinderFeatureBuilder.
SelectedGeometry
¶ Returns the selected cylinder geometry
-------------------------------------
Getter Method
Signature
SelectedGeometry
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX9.0.2.
License requirements: None.
Method Detail¶
FlipAxisDirection¶
-
InspectionCylinderFeatureBuilder.
FlipAxisDirection
¶ Flips the cylinder inspection feature axis direction vector
Signature
FlipAxisDirection()
New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UpdateAxisDirection¶
-
InspectionCylinderFeatureBuilder.
UpdateAxisDirection
¶ Updates cylinder inspection feature axis direction vector based on selected vector
Signature
UpdateAxisDirection(vector)
Parameters: vector ( NXOpen.Vector3d
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UpdateParams¶
-
InspectionCylinderFeatureBuilder.
UpdateParams
¶ Updates cylinder inspection feature characteristic parameters based on selected geometry
Signature
UpdateParams()
New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Validate¶
-
InspectionCylinderFeatureBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.