InspectionConstructedFeatureBuilderMethodEnumType Enumeration¶
NXOpen.CAM.InspectionConstructedFeatureBuilder.MethodEnumType is an alias for NXOpen.CAM.InspectionConstructedFeatureBuilderMethodEnumType
-
class
NXOpen.CAM.
InspectionConstructedFeatureBuilderMethodEnumType
¶ Bases:
object
Construction Method
Enum Members
Enum Member Enum Member Description BestFit Best Fit a feature to point reducible subfeatures Transform Transform a copy of a feature from one PCS to another PCS Intersection Intersects features to form a point plane or circle feature Minimum Finds the maximum feature measurement point in a specified direction Maximum Finds the minimum feature measurement point in a specified direction Projection Projects a measurement point onto a measured or nominal feature MoveByFeature Moves a copy of a point reducible feature in a direction associated with another feature MoveByVector Moves a copy of a point reducible feature in a user specifiec direction PerpendicularTo Creates a feature perpendicular to a feature and through another feature ParallelTo Creates a feature parallel to a feature and through another feature Offset Creates a plane or line offset by a nominal amount to each subfeature Middle Creates a point, plane or line at the middle of two sub features ConeDiameter Creates a circle at diameter of a cone ConeDistance Creates a circle at distance along a cone Extract Creates a feature by extract neasurements from other features -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-