InspectionConstructedFeatureBuilderDestPcsEnumType Enumeration¶
NXOpen.CAM.InspectionConstructedFeatureBuilder.DestPcsEnumType is an alias for NXOpen.CAM.InspectionConstructedFeatureBuilderDestPcsEnumType
-
class
NXOpen.CAM.
InspectionConstructedFeatureBuilderDestPcsEnumType
¶ Bases:
object
Specifies if the destination PCS is the current PCS or a user specified nominal or actual PCS
Enum Members
Enum Member Enum Member Description CurrentPCS Use current PCS as the destination NominalPCS Use a user specified nominal PCS as the destination ActualPCS Use a user specified actual PCS as the destination -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-