InspectionConstructedFeatureBuilderConstFeatType Enumeration¶
NXOpen.CAM.InspectionConstructedFeatureBuilder.ConstFeatType is an alias for NXOpen.CAM.InspectionConstructedFeatureBuilderConstFeatType
-
class
NXOpen.CAM.
InspectionConstructedFeatureBuilderConstFeatType
¶ Bases:
object
Type of feature to be constructed
Enum Members
Enum Member Enum Member Description Point Constructed Point Feature Line Constructed Line Feature Plane Constructed Plane Feature Arc Constructed Arc Feature Circle Constructed Circle Feature Cylinder Constructed Cylinder Feature Cone Constructed Cone Feature Sphere Constructed Sphere Feature Curve Constructed Curve Feature Torus Constructed Torus Feature Surface Constructed Surface Feature SlotTab Constructed Slot/Tab Feature -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-