InspectionAlignmentAssistantBuilderFeatureType Enumeration¶
NXOpen.CAM.InspectionAlignmentAssistantBuilder.FeatureType is an alias for NXOpen.CAM.InspectionAlignmentAssistantBuilderFeatureType
-
class
NXOpen.CAM.
InspectionAlignmentAssistantBuilderFeatureType
¶ Bases:
object
Alignment feature type
Enum Members
Enum Member Enum Member Description Plane Plane alignment feature type BestFitPlane Best Fit Plane alignment feature type OffsetPlane Offset Plane alignment feature type MidPlane Mid Plane alignment feature type Cylinder Cylinder alignment feature type BestFitCylinder Best Fit Cylinder alignment feature type Line Line alignment feature type BestFitLine Best Fit Line alignment feature type IntersectLine Intersect Line alignment feature type Circle Circle alignment feature type BestFitCircle Best Fit Circle alignment feature type Point Point alignment feature type BestFitPoint Best Fot Point alignment feature type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-