InspectionAlignmentAssistantBuilderAlignType Enumeration¶
NXOpen.CAM.InspectionAlignmentAssistantBuilder.AlignType is an alias for NXOpen.CAM.InspectionAlignmentAssistantBuilderAlignType
-
class
NXOpen.CAM.
InspectionAlignmentAssistantBuilderAlignType
¶ Bases:
object
Alignment type
Enum Members
Enum Member Enum Member Description PlanePlanePlane Plane, Plane, Plane alignment type PlaneLinePoint Plane, Line, Point alignment type PlaneCylinderCylinder Plane, Cylinder, Cylinder alignment type PlaneBoltHoleCircle Plane, Bolt Hole Circle alignment type CylinderPlanePlane Cylinder, Plane, Plane alignment type CylinderPlanePoint Cylinder, Plane, Point alignment type CylinderPlaneCylinder Cylinder, Plane, Cylinder alignment type SixPointNest Six Point Nest alignment type SPFTolerance SPF Tolerance alignment type Lsq Least Squares Best Fit alignment type Rps RPS alignment type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-