InitialProfilePlunge Class¶
-
class
NXOpen.CAM.
InitialProfilePlunge
¶ Bases:
NXOpen.TaggedObject
Represents the initial profile plunge
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
AxialCoordinate | Returns the axial coordinate |
ExtendDistance | Returns the extend distance |
Mode | Returns or sets the initial profile plunge mode |
Point | Returns or sets the initial profile plunge point |
RadialCoordinate | Returns the radial coordinate |
StopDistance | Returns the stop distance |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
InitialProfilePlungeModes Enumeration | the initial profile plunge mode |
Property Detail¶
AxialCoordinate¶
-
InitialProfilePlunge.
AxialCoordinate
¶ Returns the axial coordinate
-------------------------------------
Getter Method
Signature
AxialCoordinate
Returns: the axial builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: None.
ExtendDistance¶
-
InitialProfilePlunge.
ExtendDistance
¶ Returns the extend distance
-------------------------------------
Getter Method
Signature
ExtendDistance
Returns: the extend distance builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: None.
Mode¶
-
InitialProfilePlunge.
Mode
¶ Returns or sets the initial profile plunge mode
-------------------------------------
Getter Method
Signature
Mode
Returns: the initial profile plunge mode Return type: NXOpen.CAM.InitialProfilePlungeModes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Mode
Parameters: mode ( NXOpen.CAM.InitialProfilePlungeModes
) – the initial profile plunge modeNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
Point¶
-
InitialProfilePlunge.
Point
¶ Returns or sets the initial profile plunge point
-------------------------------------
Getter Method
Signature
Point
Returns: the initial profile plunge point Return type: NXOpen.Point
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Point
Parameters: point ( NXOpen.Point
) – the initial profile plunge pointNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
RadialCoordinate¶
-
InitialProfilePlunge.
RadialCoordinate
¶ Returns the radial coordinate
-------------------------------------
Getter Method
Signature
RadialCoordinate
Returns: the radial builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: None.
StopDistance¶
-
InitialProfilePlunge.
StopDistance
¶ Returns the stop distance
-------------------------------------
Getter Method
Signature
StopDistance
Returns: the stop distance builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: None.