InferredDouble Class¶
-
class
NXOpen.CAM.
InferredDouble
¶ Bases:
NXOpen.TaggedObject
Represents a builder for an inferred value in of a CAM.
CAMObject .. versionadded:: NX7.5.0
Properties¶
Property | Description |
---|---|
InferredStatus | Returns or sets the inferred status |
Tag | Returns the Tag for this object. |
Value | Returns or sets the current value |
Methods¶
Enumerations¶
InferredDoubleLock Enumeration | the lock statue |
Property Detail¶
InferredStatus¶
-
InferredDouble.
InferredStatus
¶ Returns or sets the inferred status
-------------------------------------
Getter Method
Signature
InferredStatus
Returns: the inferred status Return type: NXOpen.CAM.InferredDoubleLock
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InferredStatus
Parameters: isInferred ( NXOpen.CAM.InferredDoubleLock
) – the inferred statusNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
Value¶
-
InferredDouble.
Value
¶ Returns or sets the current value
-------------------------------------
Getter Method
Signature
Value
Returns: the current value Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Value
Parameters: newValue (float) – the new value New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)