HoleDrillingBuilderRetractOutputModeType Enumeration¶
NXOpen.CAM.HoleDrillingBuilder.RetractOutputModeType is an alias for NXOpen.CAM.HoleDrillingBuilderRetractOutputModeType
-
class
NXOpen.CAM.
HoleDrillingBuilderRetractOutputModeType
¶ Bases:
object
Available types for canned retract output mode
Enum Members
Enum Member Enum Member Description ClearanceOnly canned retract to clearance only ClearanceInitial canned retract to clearance and initial level Always canned retract always -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-