HoleBossGeomHoleBossTypes Enumeration¶
NXOpen.CAM.HoleBossGeom.HoleBossTypes is an alias for NXOpen.CAM.HoleBossGeomHoleBossTypes
-
class
NXOpen.CAM.
HoleBossGeomHoleBossTypes
¶ Bases:
object
the hole or boss types
New in version NX7.5.0.
Enum Members
Enum Member Enum Member Description Hole Type: Hole Boss Type: Boss ThreadedHole Type: Threaded Hole ThreadedBoss Type: Threaded Boss CenterHole Type: Center Hole ChamferHole Type: Chamfer Hole -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-