HoleBossGeomFormTypes Enumeration¶
NXOpen.CAM.HoleBossGeom.FormTypes is an alias for NXOpen.CAM.HoleBossGeomFormTypes
-
class
NXOpen.CAM.
HoleBossGeomFormTypes
¶ Bases:
object
the Form types
New in version NX7.5.0.
Enum Members
Enum Member Enum Member Description Unified Form: Unified Metric Form: Metric Trapezoidal Form: Trapezoidal Acme Form: Acme StubAcme Form: Stub Acme Lowernherz Form: Lowenherz Buttress Form: Buttress SparkPlug Form: Spark Plug Npt Form: NPT HoseCoupling Form: Hose Coupling FireHose Form: Fire Hose Unj Form: UNJ Nps Form: NPS Bsp Form: BSP Bstp Form: BSTP Helicoil Form: Helicoil Ns Form: NS UserDefined Form: User-defined -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-