GougeCheckResults Class¶
-
class
NXOpen.CAM.
GougeCheckResults
¶ Bases:
NXOpen.TransientObject
Represents the gouge results data
New in version NX11.0.2.
Properties¶
Property | Description |
---|---|
GougeOption | Returns the gouge check option |
NumberGouges | Returns the number of gouges |
NumberHolderCollisions | Returns the number of Holder Collisions |
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetGougePoints | Gouge Points |
GetHolderCollisionPoints | Holder Collision Points |
Enumerations¶
GougeCheckResultsConstants Enumeration | Constants for Gouge Results |
GougeCheckResultsOption Enumeration | Defines the gouge checking type |
Property Detail¶
GougeOption¶
-
GougeCheckResults.
GougeOption
¶ Returns the gouge check option
-------------------------------------
Getter Method
Signature
GougeOption
Returns: Return type: NXOpen.CAM.GougeCheckResultsOption
New in version NX11.0.2.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
Dispose¶
-
GougeCheckResults.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX11.0.2.
License requirements: None.
GetGougePoints¶
-
GougeCheckResults.
GetGougePoints
¶ Gouge Points
Signature
GetGougePoints()
Returns: Return type: list of NXOpen.Point3d
New in version NX11.0.2.
License requirements: cam_base (“CAM BASE”)
GetHolderCollisionPoints¶
-
GougeCheckResults.
GetHolderCollisionPoints
¶ Holder Collision Points
Signature
GetHolderCollisionPoints()
Returns: Return type: list of NXOpen.Point3d
New in version NX11.0.2.
License requirements: cam_base (“CAM BASE”)