GougeCheckBuilder Class¶
-
class
NXOpen.CAM.
GougeCheckBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAM.GougeCheckBuilder
.Which is for gouge and collision check. When
Builder.Commit()
is called None will be returned.To create a new instance of this class, use
NXOpen.CAM.CAMSetup.CreateGougeCheckBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
CheckToolAndHolder | Returns or sets the check tool and holder. |
GougeCheckStockOptions | Returns or sets the gouge check stock options. |
GougeCheckStockUserDefinedValue | Returns or sets the gouge check stock user defined value. |
PauseOnFirstGougeOrCollision | Returns or sets the pause on first gouge or collision. |
StopWhenLimitReached | Returns or sets the stop when limit reached. |
StopWhenLimitReachedMaximumLimit | Returns or sets the stop when limit reached maximum limit. |
Tag | Returns the Tag for this object. |
ToolShape | Returns or sets the tool shape. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
GougeCheckBuilderGougeCheckStock Enumeration | the gouge check stock options |
GougeCheckBuilderToolShapeType Enumeration | the tool shape options |
Property Detail¶
CheckToolAndHolder¶
-
GougeCheckBuilder.
CheckToolAndHolder
¶ Returns or sets the check tool and holder.
This is the setting for the gouge checking to check tool and holder.
-------------------------------------
Getter Method
Signature
CheckToolAndHolder
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CheckToolAndHolder
Parameters: checkToolAndHolder (bool) – New in version NX11.0.0.
License requirements: cam_base (“CAM BASE”)
GougeCheckStockOptions¶
-
GougeCheckBuilder.
GougeCheckStockOptions
¶ Returns or sets the gouge check stock options.
This is the setting for the gouge check stock options.
-------------------------------------
Getter Method
Signature
GougeCheckStockOptions
Returns: the gouge check stock options Return type: NXOpen.CAM.GougeCheckBuilderGougeCheckStock
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GougeCheckStockOptions
Parameters: options ( NXOpen.CAM.GougeCheckBuilderGougeCheckStock
) – the gouge check stock optionsNew in version NX11.0.0.
License requirements: cam_base (“CAM BASE”)
GougeCheckStockUserDefinedValue¶
-
GougeCheckBuilder.
GougeCheckStockUserDefinedValue
¶ Returns or sets the gouge check stock user defined value.
This is the setting when user selects user defined gouge check stock.
-------------------------------------
Getter Method
Signature
GougeCheckStockUserDefinedValue
Returns: the gouge check stock user defined value Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GougeCheckStockUserDefinedValue
Parameters: userDefinedValue (float) – the gouge check stock user defined value New in version NX11.0.0.
License requirements: cam_base (“CAM BASE”)
PauseOnFirstGougeOrCollision¶
-
GougeCheckBuilder.
PauseOnFirstGougeOrCollision
¶ Returns or sets the pause on first gouge or collision.
This is the options to stop the gouge checking when encounter first gouge.
-------------------------------------
Getter Method
Signature
PauseOnFirstGougeOrCollision
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PauseOnFirstGougeOrCollision
Parameters: pauseOnFirstGougeOrCollision (bool) – New in version NX11.0.0.
License requirements: cam_base (“CAM BASE”)
StopWhenLimitReached¶
-
GougeCheckBuilder.
StopWhenLimitReached
¶ Returns or sets the stop when limit reached.
This is the options to stop or continue the gouge checking when encounter any gouge.
-------------------------------------
Getter Method
Signature
StopWhenLimitReached
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StopWhenLimitReached
Parameters: stopWhenLimitReached (bool) – New in version NX11.0.0.
License requirements: cam_base (“CAM BASE”)
StopWhenLimitReachedMaximumLimit¶
-
GougeCheckBuilder.
StopWhenLimitReachedMaximumLimit
¶ Returns or sets the stop when limit reached maximum limit.
The gouge checking will be stopped when reached the maximum limit.
-------------------------------------
Getter Method
Signature
StopWhenLimitReachedMaximumLimit
Returns: Return type: int New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StopWhenLimitReachedMaximumLimit
Parameters: maximumLimit (int) – New in version NX11.0.0.
License requirements: cam_base (“CAM BASE”)
ToolShape¶
-
GougeCheckBuilder.
ToolShape
¶ Returns or sets the tool shape.
This is the setting for which tool shape type is used for the gouge checking.
-------------------------------------
Getter Method
Signature
ToolShape
Returns: the tool shape type Return type: NXOpen.CAM.GougeCheckBuilderToolShapeType
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToolShape
Parameters: type ( NXOpen.CAM.GougeCheckBuilderToolShapeType
) – the tool shape typeNew in version NX11.0.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
Validate¶
-
GougeCheckBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.