GeometrySetMaterialSideTypes Enumeration¶
NXOpen.CAM.GeometrySet.MaterialSideTypes is an alias for NXOpen.CAM.GeometrySetMaterialSideTypes
-
class
NXOpen.CAM.
GeometrySetMaterialSideTypes
¶ Bases:
object
Available types for Material Side
New in version NX8.0.0.
Enum Members
Enum Member Enum Member Description NotSet none Same the tool is cutting on the same side as the natural side of the entity Opposite the tool cuts the opposite side -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-