GeometrySetLoopsIgnoreTypes Enumeration¶
NXOpen.CAM.GeometrySet.LoopsIgnoreTypes is an alias for NXOpen.CAM.GeometrySetLoopsIgnoreTypes
-
class
NXOpen.CAM.
GeometrySetLoopsIgnoreTypes
¶ Bases:
object
Available types for Ignore Loops
New in version NX8.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.Features.PatchOpeningsBuilder
instead.Enum Members
Enum Member Enum Member Description NotSet none All all Specify specify -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-