GeometryGroupPositionTypes Enumeration¶
NXOpen.CAM.GeometryGroup.PositionTypes is an alias for NXOpen.CAM.GeometryGroupPositionTypes
-
class
NXOpen.CAM.
GeometryGroupPositionTypes
¶ Bases:
object
the ipw position types
Enum Members
Enum Member Enum Member Description Part ipw position using part Coordinate ipw position using coordinate system -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-