GeometryGroupBlankDefinitionTypes Enumeration¶
NXOpen.CAM.GeometryGroup.BlankDefinitionTypes is an alias for NXOpen.CAM.GeometryGroupBlankDefinitionTypes
-
class
NXOpen.CAM.
GeometryGroupBlankDefinitionTypes
¶ Bases:
object
the blank definition types
Enum Members
Enum Member Enum Member Description FromGeometry blank defined through selected geometry OffsetFromPart blank defined through offset from part AutoBlock blank defined through auto block around part Ipw blank defined through IPW BoundingCylinder blank defined through bounding cylinder PartOutline blank defined through part outline PartConvexHull blank defined through part convex hull -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-