FollowPartMoveBuilderMoveDirectionTypes Enumeration

NXOpen.CAM.FollowPartMoveBuilder.MoveDirectionTypes is an alias for NXOpen.CAM.FollowPartMoveBuilderMoveDirectionTypes

class NXOpen.CAM.FollowPartMoveBuilderMoveDirectionTypes

Bases: object

Available types for manual move path direction in GMC operation

Enum Members

Enum Member Enum Member Description
Undefined
Forward
Reverse
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.