FlowCutSteepContainmentSteepCutDirectionTypes Enumeration

NXOpen.CAM.FlowCutSteepContainment.SteepCutDirectionTypes is an alias for NXOpen.CAM.FlowCutSteepContainmentSteepCutDirectionTypes

class NXOpen.CAM.FlowCutSteepContainmentSteepCutDirectionTypes

Bases: object

Available types for Steep Cut Direct in Flow Cut

Enum Members

Enum Member Enum Member Description
Mixed Mixed
HighToLow High to Low
LowToHigh Low to High
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.