FinishDwell Class¶
-
class
NXOpen.CAM.
FinishDwell
¶ Bases:
NXOpen.TaggedObject
Represents a
NXOpen.CAM.FinishDwell
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
Type | Returns or sets the dwell after finish/profile cut mode |
Value | Returns or sets the dwell after finish/profile cut |
Methods¶
Enumerations¶
FinishDwellTypes Enumeration | The dwell after finish/profile cut mode options |
Property Detail¶
Type¶
-
FinishDwell.
Type
¶ Returns or sets the dwell after finish/profile cut mode
-------------------------------------
Getter Method
Signature
Type
Returns: the dwell after finish/profile cut mode Return type: NXOpen.CAM.FinishDwellTypes
New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
Type
Parameters: dwellMode ( NXOpen.CAM.FinishDwellTypes
) – the dwell after finish/profile cut modeNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
Value¶
-
FinishDwell.
Value
¶ Returns or sets the dwell after finish/profile cut
-------------------------------------
Getter Method
Signature
Value
Returns: the dwell after finish/profile cut Return type: float New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
Value
Parameters: dwellValue (float) – the dwell after finish/profile cut New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)