FeedsBuilderRecalcuateBasedOn Enumeration¶
NXOpen.CAM.FeedsBuilder.RecalcuateBasedOn is an alias for NXOpen.CAM.FeedsBuilderRecalcuateBasedOn
-
class
NXOpen.CAM.
FeedsBuilderRecalcuateBasedOn
¶ Bases:
object
The recalculation based on attribute
New in version NX8.0.0.
Enum Members
Enum Member Enum Member Description SurfaceSpeed surface speed SpindleSpeed spindle speed FeedPerTooth feed per tooth CutFeedRate cut feed rate -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-