FeatureRecognitionBuilderRecognitionEnum Enumeration¶
NXOpen.CAM.FeatureRecognitionBuilder.RecognitionEnum is an alias for NXOpen.CAM.FeatureRecognitionBuilderRecognitionEnum
-
class
NXOpen.CAM.
FeatureRecognitionBuilderRecognitionEnum
¶ Bases:
object
the type of feature search
Enum Members
Enum Member Enum Member Description Identify Feature Identification from modeling features Parametric Parametric Feature Recognition Legacy Legacy Hole Feature Recognition Generic Legacy Face and Pocket Feature Recognition Manual Manual Feature Recognition -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-