FeatureRecognitionBuilderGeometrySearch Enumeration¶
NXOpen.CAM.FeatureRecognitionBuilder.GeometrySearch is an alias for NXOpen.CAM.FeatureRecognitionBuilderGeometrySearch
-
class
NXOpen.CAM.
FeatureRecognitionBuilderGeometrySearch
¶ Bases:
object
the geometry search type
Enum Members
Enum Member Enum Member Description Workpiece Search for features in workpiece AllGeometry Search for features in all geometry Selected Search for features in user-selected geometry -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-