FeatureGeometryGroupProcessStatus Enumeration¶
NXOpen.CAM.FeatureGeometryGroup.ProcessStatus is an alias for NXOpen.CAM.FeatureGeometryGroupProcessStatus
-
class
NXOpen.CAM.
FeatureGeometryGroupProcessStatus
¶ Bases:
object
Update status of the feature
Enum Members
Enum Member Enum Member Description Unknown Feature group status is unknown Ok Feature group status is ok Suspect Feature group status is suspected -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-