FacesSequenceTypes Enumeration¶
NXOpen.CAM.FacesSequence.Types is an alias for NXOpen.CAM.FacesSequenceTypes
-
class
NXOpen.CAM.
FacesSequenceTypes
¶ Bases:
object
The faces sequence options
New in version NX6.0.0.
Enum Members
Enum Member Enum Member Description SameAsFacesDiameters Faces Sequence: Same As Faces/Diameters Reversed Faces Sequence: Reversed -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-