ThreadFeatureGeometryForm Enumeration¶
NXOpen.CAM.FBM.ThreadFeatureGeometry.Form is an alias for NXOpen.CAM.FBM.ThreadFeatureGeometryForm
-
class
NXOpen.CAM.FBM.
ThreadFeatureGeometryForm
¶ Bases:
object
Thread form standards
New in version NX9.0.2.
Enum Members
Enum Member Enum Member Description Unified Form: Unified Acme Form: Acme StubAcme Form: Stub Acme Buttress Form: Buttress Metric Form: Metric Trapezoidal Form: Trapezoidal Lowernherz Form: Lowenherz SparkPlug Form: Spark Plug Npt Form: NPT HoseCoupling Form: Hose Coupling FireHose Form: Fire Hose Unj Form: UNJ Nps Form: NPS Bsp Form: BSP Bstp Form: BSTP Helicoil Form: Helicoil Ns Form: NS UserDefined Form: User defined -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-