ElementIntBuilder Class¶
-
class
NXOpen.CAM.
ElementIntBuilder
¶ Bases:
NXOpen.TaggedObject
Represents a builder for an Element int value in of a CAM.
CAMObject .. versionadded:: NX10.0.1
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
Value | Returns or sets the current value |
Methods¶
Property Detail¶
Value¶
-
ElementIntBuilder.
Value
¶ Returns or sets the current value
-------------------------------------
Getter Method
Signature
Value
Returns: the current value Return type: int New in version NX10.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
Value
Parameters: newValue (int) – the new value New in version NX10.0.1.
License requirements: cam_base (“CAM BASE”)