DriveModeType Enumeration

NXOpen.CAM.DriveMode.Type is an alias for NXOpen.CAM.DriveModeType

class NXOpen.CAM.DriveModeType

Bases: object

Available types for Drive Mode

New in version NX7.5.0.

Enum Members

Enum Member Enum Member Description
LowerBlendEdge Lower Blend Edge
ReferenceTool Reference Tool
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.