DrillThreadMillToolBuilderToolFormTypeTypes Enumeration¶
NXOpen.CAM.DrillThreadMillToolBuilder.ToolFormTypeTypes is an alias for NXOpen.CAM.DrillThreadMillToolBuilderToolFormTypeTypes
-
class
NXOpen.CAM.
DrillThreadMillToolBuilderToolFormTypeTypes
¶ Bases:
object
form type
Enum Members
Enum Member Enum Member Description Unified Unified Metric Metric Trapezoidal Trapezoidal Acme Acme Stubacme Stub Acme Lowenherz Lowenherz Buttress Buttress Sparkplug Spark Plug Npt NPT Hosecoupling Hose Coupling Firehose Fire Hose Unj UNJ Nps NPS Bsp BSP Bstp BSTP Helicoil Helicoil Ns NS UserDefined User Defined -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-