DmToolPosition Class¶
-
class
NXOpen.CAM.
DmToolPosition
¶ Bases:
NXOpen.TaggedObject
Represents a streamline tool position builder
This is an abstract class and cannot be instantiated.
New in version NX10.0.1.
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
ToolPosition | Returns or sets the tool position |
ToolPositionType | Returns or sets the tool position used for common block |
Methods¶
Enumerations¶
DmToolPositionToolPositionOption Enumeration | Enum of tool position |
Property Detail¶
ToolPosition¶
-
DmToolPosition.
ToolPosition
¶ Returns or sets the tool position
-------------------------------------
Getter Method
Signature
ToolPosition
Returns: the tool position value Return type: NXOpen.CAM.DPMItpBuilderToolPositionOption
New in version NX10.0.1.
Deprecated since version NX11.0.1: Please use
NXOpen.CAM.DmToolPosition.ToolPositionType()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
ToolPosition
Parameters: toolPosition ( NXOpen.CAM.DPMItpBuilderToolPositionOption
) – the tool position valueNew in version NX10.0.1.
Deprecated since version NX11.0.1: Please use
NXOpen.CAM.DmToolPosition.ToolPositionType()
instead.License requirements: cam_base (“CAM BASE”)
ToolPositionType¶
-
DmToolPosition.
ToolPositionType
¶ Returns or sets the tool position used for common block
-------------------------------------
Getter Method
Signature
ToolPositionType
Returns: the tool position value Return type: NXOpen.CAM.DmToolPositionToolPositionOption
New in version NX11.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToolPositionType
Parameters: toolPosition ( NXOpen.CAM.DmToolPositionToolPositionOption
) – the tool position valueNew in version NX11.0.1.
License requirements: cam_base (“CAM BASE”)