DmSurfBuilderToolPositionType Enumeration

NXOpen.CAM.DmSurfBuilder.ToolPositionType is an alias for NXOpen.CAM.DmSurfBuilderToolPositionType

class NXOpen.CAM.DmSurfBuilderToolPositionType

Bases: object

Available types for SDM: Tool Position Type

Enum Members

Enum Member Enum Member Description
On On
Tanto Tanto
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.