DmSurfBuilderMatSideType Enumeration

NXOpen.CAM.DmSurfBuilder.MatSideType is an alias for NXOpen.CAM.DmSurfBuilderMatSideType

class NXOpen.CAM.DmSurfBuilderMatSideType

Bases: object

Available types for Flip Material, SDM: Select Cut Direction

Enum Members

Enum Member Enum Member Description
Same same
Opp opp
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.