DmSurfBuilderDmSurfCutStepType Enumeration

NXOpen.CAM.DmSurfBuilder.DmSurfCutStepType is an alias for NXOpen.CAM.DmSurfBuilderDmSurfCutStepType

class NXOpen.CAM.DmSurfBuilderDmSurfCutStepType

Bases: object

Available types for SDM: Cut Step

Enum Members

Enum Member Enum Member Description
Tolerance Tolerances
Points Number
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.