DmSurfBuilderCutDirection Enumeration

NXOpen.CAM.DmSurfBuilder.CutDirection is an alias for NXOpen.CAM.DmSurfBuilderCutDirection

class NXOpen.CAM.DmSurfBuilderCutDirection

Bases: object

Available types for Cut Direction

Enum Members

Enum Member Enum Member Description
Corner1U Corner 1 U direction
Corner1V Corner 1 V direction
Corner2U Corner 2 U direction
Corner2V Corner 2 V direction
Corner3U Corner 3 U direction
Corner3V Corner 3 V direction
Corner4U Corner 4 U direction
Corner4V Corner 4 V direction
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.