DmRotaryFloorFinishBuilderMatSideType Enumeration

NXOpen.CAM.DmRotaryFloorFinishBuilder.MatSideType is an alias for NXOpen.CAM.DmRotaryFloorFinishBuilderMatSideType

class NXOpen.CAM.DmRotaryFloorFinishBuilderMatSideType

Bases: object

the types for flip material

Enum Members

Enum Member Enum Member Description
Same same
Opp opp
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.