DmRotaryFloorFinishBuilderDmSurfCutAreaType Enumeration

NXOpen.CAM.DmRotaryFloorFinishBuilder.DmSurfCutAreaType is an alias for NXOpen.CAM.DmRotaryFloorFinishBuilderDmSurfCutAreaType

class NXOpen.CAM.DmRotaryFloorFinishBuilderDmSurfCutAreaType

Bases: object

the types for cut area

Enum Members

Enum Member Enum Member Description
SurfacePercent Surface %
DiagonalPoints Diagonal Points
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.