DmRotaryFloorFinishBuilderDirectionType Enumeration

NXOpen.CAM.DmRotaryFloorFinishBuilder.DirectionType is an alias for NXOpen.CAM.DmRotaryFloorFinishBuilderDirectionType

class NXOpen.CAM.DmRotaryFloorFinishBuilderDirectionType

Bases: object

the types for direction

Enum Members

Enum Member Enum Member Description
AroundAxis around axis
AlongAxis along axis
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.