DmRadBuilderRadTraverseDirType Enumeration

NXOpen.CAM.DmRadBuilder.RadTraverseDirType is an alias for NXOpen.CAM.DmRadBuilderRadTraverseDirType

class NXOpen.CAM.DmRadBuilderRadTraverseDirType

Bases: object

Available types for Radial Cut/ Traverse Direction

Enum Members

Enum Member Enum Member Description
Forward Follow Boundary
Backward Reverse Boundary
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.