DmRadBuilderRadStepoverTypeType Enumeration¶
NXOpen.CAM.DmRadBuilder.RadStepoverTypeType is an alias for NXOpen.CAM.DmRadBuilderRadStepoverTypeType
-
class
NXOpen.CAM.
DmRadBuilderRadStepoverTypeType
¶ Bases:
object
Available types for Stepover for the Radial Cut in scop. The enum type is obsolete.
Enum Members
Enum Member Enum Member Description Constant Constant Scallop Scallop Tool Tool Diameter Maximum Maximum -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-