DmCmMultiplePassesCiBuilderOrderType Enumeration

NXOpen.CAM.DmCmMultiplePassesCiBuilder.OrderType is an alias for NXOpen.CAM.DmCmMultiplePassesCiBuilderOrderType

class NXOpen.CAM.DmCmMultiplePassesCiBuilderOrderType

Bases: object

Available types for Order

Enum Members

Enum Member Enum Member Description
WallFirst Wall First
FloorFirst Floor First
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.