DmCmBuilderToolAxisGuideVectorType Enumeration

NXOpen.CAM.DmCmBuilder.ToolAxisGuideVectorType is an alias for NXOpen.CAM.DmCmBuilderToolAxisGuideVectorType

class NXOpen.CAM.DmCmBuilderToolAxisGuideVectorType

Bases: object

Available types for vector type, Contour Milling Drive

Enum Members

Enum Member Enum Member Description
Auto automatic
Guide user specified
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.