DmCmBuilderExtDisType Enumeration

NXOpen.CAM.DmCmBuilder.ExtDisType is an alias for NXOpen.CAM.DmCmBuilderExtDisType

class NXOpen.CAM.DmCmBuilderExtDisType

Bases: object

Available types for ext_dis, Contour Milling Drive: Start of Cut

Enum Members

Enum Member Enum Member Description
NotSet None
Fixed Specify
Percent Tool Diameter
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.