DmCmBuilderContactPositionRingHeightType Enumeration

NXOpen.CAM.DmCmBuilder.ContactPositionRingHeightType is an alias for NXOpen.CAM.DmCmBuilderContactPositionRingHeightType

class NXOpen.CAM.DmCmBuilderContactPositionRingHeightType

Bases: object

Available types for contact position ring height

Enum Members

Enum Member Enum Member Description
NotSet none
Constant constant
Variable variable
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.