DmBndBuilderBndCutPatternTypes Enumeration¶
NXOpen.CAM.DmBndBuilder.BndCutPatternTypes is an alias for NXOpen.CAM.DmBndBuilderBndCutPatternTypes
-
class
NXOpen.CAM.
DmBndBuilderBndCutPatternTypes
¶ Bases:
object
Available types for Boundary cut pattern in FASurfaceContour
Enum Members
Enum Member Enum Member Description FollowPeriphery Follow Periphery Profile Profile Sep1 separate one ParallelLines Parallel Lines RadialLines Radial Lines ConcArcs Concentric Arcs Sep2 separate two StandardDrive Standard Drive -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-