DmAmBuilderSteepOptTypes Enumeration

NXOpen.CAM.DmAmBuilder.SteepOptTypes is an alias for NXOpen.CAM.DmAmBuilderSteepOptTypes

class NXOpen.CAM.DmAmBuilderSteepOptTypes

Bases: object

Available types for area milling Steep Option

Enum Members

Enum Member Enum Member Description
SteepContainNone
NonSteepNonDirectional
SteepDirectional
SteepAndNonsteep
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.