DmAmBuilderAmCutTraversalTypes Enumeration¶
NXOpen.CAM.DmAmBuilder.AmCutTraversalTypes is an alias for NXOpen.CAM.DmAmBuilderAmCutTraversalTypes
-
class
NXOpen.CAM.
DmAmBuilderAmCutTraversalTypes
¶ Bases:
object
Available types for Area Milling cut traversal in FASurfaceContour
Enum Members
Enum Member Enum Member Description ZigZag Zig-Zag ZigZagWithLifts Zig-Zag with Lifts Zig Zig Contour Zig with Contour Stepover Zig with Stepover -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-