DisplayTool Class¶
-
class
NXOpen.CAM.
DisplayTool
¶ Bases:
NXOpen.TaggedObject
Represents a display tool Builder
This is an abstract class and cannot be instantiated.
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
ToolDisplayFrequency | Returns or sets the tool display frequency |
ToolDisplayType | Returns or sets the tool display types |
Methods¶
Enumerations¶
DisplayToolToolDisplayTypes Enumeration | the tool display types |
Property Detail¶
ToolDisplayFrequency¶
-
DisplayTool.
ToolDisplayFrequency
¶ Returns or sets the tool display frequency
-------------------------------------
Getter Method
Signature
ToolDisplayFrequency
Returns: the tool display frequency Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToolDisplayFrequency
Parameters: toolDisplayFrequency (int) – the tool display frequency New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
ToolDisplayType¶
-
DisplayTool.
ToolDisplayType
¶ Returns or sets the tool display types
-------------------------------------
Getter Method
Signature
ToolDisplayType
Returns: the tool display type Return type: NXOpen.CAM.DisplayToolToolDisplayTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToolDisplayType
Parameters: toolDisplay ( NXOpen.CAM.DisplayToolToolDisplayTypes
) – the tool display typeNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)