DisplaySilhouette Class¶
-
class
NXOpen.CAM.
DisplaySilhouette
¶ Bases:
NXOpen.TaggedObject
Represents a display silhouette Builder
This is an abstract class and cannot be instantiated.
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
PercentOfTool | Returns or sets the percent of tool. |
Tag | Returns the Tag for this object. |
Methods¶
Property Detail¶
PercentOfTool¶
-
DisplaySilhouette.
PercentOfTool
¶ Returns or sets the percent of tool.
The range is 1-100.
-------------------------------------
Getter Method
Signature
PercentOfTool
Returns: the percent of tool.The range is 1-100. Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PercentOfTool
Parameters: percentTool (float) – the percent of tool.The range is 1-100. New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)